ACTION#.CONDITION

Description

This keyword defines the condition to test the action source for. If the value is 0 (always), then no test is performed and the condition always passes.

The available values of this parameter depend on the value of ACTION#.SOURCE. If the source is changed, the available range may be updated and the condition will be reset to default. Available conditions are:

Value Description
0 Always passes
1 Is false
2 Is true
3 Less than
4 Greater than
5 Rising Edge
6 Falling Edge
7 Rises above threshold
8 Falls below threshold
9 Rising Edge (triggers on high at start)
10 Falling Edge (triggers on low at start)
11 Is Equal To
12 Becomes Equal To

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.SOURCE

Default Value

0 (always)

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

ACTION1.CONDITION

3901h

01h

Unsigned8

-

-

Read/Write

No

ACTION2.CONDITION

3901h

02h

Unsigned8

-

-

Read/Write

No

ACTION3.CONDITION

3901h

03h

Unsigned8

-

-

Read/Write

No

ACTION4.CONDITION

3901h

04h

Unsigned8

-

-

Read/Write

No

ACTION5.CONDITION

3901h

05h

Unsigned8

-

-

Read/Write

No

ACTION6.CONDITION

3901h

06h

Unsigned8

-

-

Read/Write

No

ACTION7.CONDITION

3901h

07h

Unsigned8

-

-

Read/Write

No

ACTION8.CONDITION

3901h

08h

Unsigned8

-

-

Read/Write

No

ACTION9.CONDITION

3901h

09h

Unsigned8

-

-

Read/Write

No

ACTION10.CONDITION

3901h

0ah

Unsigned8

-

-

Read/Write

No

ACTION11.CONDITION

3901h

0bh

Unsigned8

-

-

Read/Write

No

ACTION12.CONDITION

3901h

0ch

Unsigned8

-

-

Read/Write

No

ACTION13.CONDITION

3901h

0dh

Unsigned8

-

-

Read/Write

No

ACTION14.CONDITION

3901h

0eh

Unsigned8

-

-

Read/Write

No

ACTION15.CONDITION

3901h

0fh

Unsigned8

-

-

Read/Write

No

ACTION16.CONDITION

3901h

10h

Unsigned8

-

-

Read/Write

No

ACTION17.CONDITION

3901h

11h

Unsigned8

-

-

Read/Write

No

ACTION18.CONDITION

3901h

12h

Unsigned8

-

-

Read/Write

No

ACTION19.CONDITION

3901h

13h

Unsigned8

-

-

Read/Write

No

ACTION20.CONDITION

3901h

14h

Unsigned8

-

-

Read/Write

No

ACTION21.CONDITION

3901h

15h

Unsigned8

-

-

Read/Write

No

ACTION22.CONDITION

3901h

16h

Unsigned8

-

-

Read/Write

No

ACTION23.CONDITION

3901h

17h

Unsigned8

-

-

Read/Write

No

ACTION24.CONDITION

3901h

18h

Unsigned8

-

-

Read/Write

No

ACTION25.CONDITION

3901h

19h

Unsigned8

-

-

Read/Write

No

ACTION26.CONDITION

3901h

1ah

Unsigned8

-

-

Read/Write

No

ACTION27.CONDITION

3901h

1bh

Unsigned8

-

-

Read/Write

No

ACTION28.CONDITION

3901h

1ch

Unsigned8

-

-

Read/Write

No

ACTION29.CONDITION

3901h

1dh

Unsigned8

-

-

Read/Write

No

ACTION30.CONDITION

3901h

1eh

Unsigned8

-

-

Read/Write

No

ACTION31.CONDITION

3901h

1fh

Unsigned8

-

-

Read/Write

No

ACTION32.CONDITION

3901h

20h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

40200

1

40200 (0x9d08)

ACTION1.CONDITION

Unsigned8

Read/Write

Yes

40201

1

40201 (0x9d09)

ACTION2.CONDITION

Unsigned8

Read/Write

Yes

40202

1

40202 (0x9d0a)

ACTION3.CONDITION

Unsigned8

Read/Write

Yes

40203

1

40203 (0x9d0b)

ACTION4.CONDITION

Unsigned8

Read/Write

Yes

40204

1

40204 (0x9d0c)

ACTION5.CONDITION

Unsigned8

Read/Write

Yes

40205

1

40205 (0x9d0d)

ACTION6.CONDITION

Unsigned8

Read/Write

Yes

40206

1

40206 (0x9d0e)

ACTION7.CONDITION

Unsigned8

Read/Write

Yes

40207

1

40207 (0x9d0f)

ACTION8.CONDITION

Unsigned8

Read/Write

Yes

40208

1

40208 (0x9d10)

ACTION9.CONDITION

Unsigned8

Read/Write

Yes

40209

1

40209 (0x9d11)

ACTION10.CONDITION

Unsigned8

Read/Write

Yes

40210

1

40210 (0x9d12)

ACTION11.CONDITION

Unsigned8

Read/Write

Yes

40211

1

40211 (0x9d13)

ACTION12.CONDITION

Unsigned8

Read/Write

Yes

40212

1

40212 (0x9d14)

ACTION13.CONDITION

Unsigned8

Read/Write

Yes

40213

1

40213 (0x9d15)

ACTION14.CONDITION

Unsigned8

Read/Write

Yes

40214

1

40214 (0x9d16)

ACTION15.CONDITION

Unsigned8

Read/Write

Yes

40215

1

40215 (0x9d17)

ACTION16.CONDITION

Unsigned8

Read/Write

Yes

40216

1

40216 (0x9d18)

ACTION17.CONDITION

Unsigned8

Read/Write

Yes

40217

1

40217 (0x9d19)

ACTION18.CONDITION

Unsigned8

Read/Write

Yes

40218

1

40218 (0x9d1a)

ACTION19.CONDITION

Unsigned8

Read/Write

Yes

40219

1

40219 (0x9d1b)

ACTION20.CONDITION

Unsigned8

Read/Write

Yes

40220

1

40220 (0x9d1c)

ACTION21.CONDITION

Unsigned8

Read/Write

Yes

40221

1

40221 (0x9d1d)

ACTION22.CONDITION

Unsigned8

Read/Write

Yes

40222

1

40222 (0x9d1e)

ACTION23.CONDITION

Unsigned8

Read/Write

Yes

40223

1

40223 (0x9d1f)

ACTION24.CONDITION

Unsigned8

Read/Write

Yes

40224

1

40224 (0x9d20)

ACTION25.CONDITION

Unsigned8

Read/Write

Yes

40225

1

40225 (0x9d21)

ACTION26.CONDITION

Unsigned8

Read/Write

Yes

40226

1

40226 (0x9d22)

ACTION27.CONDITION

Unsigned8

Read/Write

Yes

40227

1

40227 (0x9d23)

ACTION28.CONDITION

Unsigned8

Read/Write

Yes

40228

1

40228 (0x9d24)

ACTION29.CONDITION

Unsigned8

Read/Write

Yes

40229

1

40229 (0x9d25)

ACTION30.CONDITION

Unsigned8

Read/Write

Yes

40230

1

40230 (0x9d26)

ACTION31.CONDITION

Unsigned8

Read/Write

Yes

40231

1

40231 (0x9d27)

ACTION32.CONDITION

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.CONDITION

40200

Unsigned8

Read/Write

-

ACTION2.CONDITION

40201

Unsigned8

Read/Write

-

ACTION3.CONDITION

40202

Unsigned8

Read/Write

-

ACTION4.CONDITION

40203

Unsigned8

Read/Write

-

ACTION5.CONDITION

40204

Unsigned8

Read/Write

-

ACTION6.CONDITION

40205

Unsigned8

Read/Write

-

ACTION7.CONDITION

40206

Unsigned8

Read/Write

-

ACTION8.CONDITION

40207

Unsigned8

Read/Write

-

ACTION9.CONDITION

40208

Unsigned8

Read/Write

-

ACTION10.CONDITION

40209

Unsigned8

Read/Write

-

ACTION11.CONDITION

40210

Unsigned8

Read/Write

-

ACTION12.CONDITION

40211

Unsigned8

Read/Write

-

ACTION13.CONDITION

40212

Unsigned8

Read/Write

-

ACTION14.CONDITION

40213

Unsigned8

Read/Write

-

ACTION15.CONDITION

40214

Unsigned8

Read/Write

-

ACTION16.CONDITION

40215

Unsigned8

Read/Write

-

ACTION17.CONDITION

40216

Unsigned8

Read/Write

-

ACTION18.CONDITION

40217

Unsigned8

Read/Write

-

ACTION19.CONDITION

40218

Unsigned8

Read/Write

-

ACTION20.CONDITION

40219

Unsigned8

Read/Write

-

ACTION21.CONDITION

40220

Unsigned8

Read/Write

-

ACTION22.CONDITION

40221

Unsigned8

Read/Write

-

ACTION23.CONDITION

40222

Unsigned8

Read/Write

-

ACTION24.CONDITION

40223

Unsigned8

Read/Write

-

ACTION25.CONDITION

40224

Unsigned8

Read/Write

-

ACTION26.CONDITION

40225

Unsigned8

Read/Write

-

ACTION27.CONDITION

40226

Unsigned8

Read/Write

-

ACTION28.CONDITION

40227

Unsigned8

Read/Write

-

ACTION29.CONDITION

40228

Unsigned8

Read/Write

-

ACTION30.CONDITION

40229

Unsigned8

Read/Write

-

ACTION31.CONDITION

40230

Unsigned8

Read/Write

-

ACTION32.CONDITION

40231

Unsigned8

Read/Write

-